Industry Online Support
Technical Forum
11/8/2009 8:45 AM | |
Posts: 7 Rating: (1) |
Hi Is STEP7 Working Properly and it's Passable to Install to Microsoft Windows 7? |
11/8/2009 8:51 AM | |
Posts: 160 Rating: (16) |
Hi, Refer below for the compatability of Step 7 with Windows OS http://support.automation.siemens.com/WW/view/en/22644954 As shown Windows 7 is not yet compatabile. This does not mean it won't work it just means it hasn't been tested yet. If in doubt try the compatability mode of Windows 7. |
11/8/2009 9:22 AM | |
Posts: 7 Rating: (1) |
Hi Again. when I Try To Install STEP 7 on Windows 7 OS I got The Messeg That it can't Install The Softwere Because Of Compatibility. So, What I Should do? |
11/8/2009 11:34 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating: (110) |
Hi nir_bb, please have a look at this thread: Windows 7 I would allways prefere a operating system were the compatibility is tested good luck Sabine |
11/9/2009 6:51 AM | |
Posts: 382 Rating: (47) |
Hi, Check out this links for your version of step7 with OS compatibility. 1] link1 2] link2 Hope this helps! with regards, how come |
11/9/2009 10:05 AM | |
Joined: 4/24/2009 Last visit: 7/18/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the thread with the subject Windows 7 Best regards O_Moderator |
Follow us on