12/21/2007 10:04 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
Hi, It could be that the CPU102 is in the fast mode, then it works 10 times as fast as normal.... Please look in the handbook of the S5-100U for further information. Handbook S5-100U: 1091978 6ES5998-0UB23 S5-100U Programmable Controller E04 See the pages 4-5 en 4-6 for more information |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/17/2008 7:11 AM | |
Posts: 9 Rating: (0) |
Yes it is CPU102, but if we need to change, the whole PLC will probably be changed to the S7-200 instead. |
1/17/2008 7:33 PM | |
Joined: 2/27/2007 Last visit: 3/30/2022 Posts: 79 Rating: (5) |
Thats good. I think it is better to change to S7-200 |
12/1/2016 12:43 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by fractalkaos is split to a separate thread with the subject Change cpu to 102 fast mode. Best regards |