8/25/2009 7:03 PM | |
Posts: 7 Rating:
|
hi, i want to connect with plc5.for online connection with plc which steps are required in step5.any body guide me. |
8/25/2009 10:17 PM | |
Posts: 2661 Rating:
|
Hi johan immi, I am a bit confused... Do you want to connect SIMATIC S5 PLC to AB PLC5? Regards |
8/27/2009 11:03 PM | |
Posts: 7 Rating:
|
connect with field pg with winxp.pg setting is ok but step setting to connect program online with plc |
8/28/2009 7:13 PM | |
Posts: 2661 Rating:
|
Do you mean Set PG/PC Interfacesetting?This will be MPI orProfibus or ISO Ind. Ethernet etc. depending on how you want to communicate with the PLC... P.S. Are you talking about S5 or S7? If S7 following link may be helpful: How can you set up the online connection again between the PG and the CPU? |
Last edited by: Phantom75 at: 8/28/2009 11:57 PMADDED P.S. |
|
8/29/2009 6:51 PM | |
Posts: 7 Rating:
|
THANKS FOR REPLYING.I WANT TO CONNECT 115U CPU WITH PG AND I WANT TO KNOW STEP5 SOTFWARE CONFIGURATION. |
This contribution was helpful to
1 thankful Users |
8/29/2009 9:32 PM | |
Posts: 1 Rating:
|
i suggest you to read the manual for program and if you have a pg the computer has diferent buttons so use the proper manual for your program http://support.automation.siemens.com/WW/view/en/9830806 look att capter 3 User Interace |
This contribution was helpful to
1 thankful Users |
Follow us on