1/3/2018 1:25 PM | |
Joined: 10/11/2017 Last visit: 3/21/2022 Posts: 32 Rating: (1) |
Dear all, I am using a 414-5 H PN/DP (redundant) CPU to which a few ET200SP modules are attached. I have two questions. 1) [snip] ... 2) I am looking for a diagnostic function (in Step 7, STL) that gives me the (diagnostic) state of a channel (the red marked component on the attached image). A function that gives me the exact address of such a red component in case it encounters something like a wire break or another error. Is there someone that would want to help me with this issue? Thank you in advance. Kind Regards. ---------------------- |
Last edited by: CS Moderator at: 1/6/2018 11:32:27 AMseperated into two threads |
|
1/9/2018 9:56 AM | |
Joined: 10/11/2017 Last visit: 3/21/2022 Posts: 32 Rating: (1) |
This is exactly what I've been looking for. It works perfectly! Thank you so much :) |