9/21/2008 12:08 PM | |
Posts: 7 Rating: (0) |
Hello, How can I download STEP7 Version 5.4. I need CPU 414-2XK05-0AB0 GSD file. Thank you very much
|
9/21/2008 12:49 PM | |
Joined: 9/27/2006 Last visit: 4/28/2024 Posts: 12257 Rating: (2665) |
Hello Siemens Users; Are you sure you want a gsd file for that CPU? Do you plan on inserting it as a Profibus-DP slave in a network? in that case, look at the following link, it providesa download for gsd files for Simatic CPUs: http://support.automation.siemens.com/WW/view/en/113652 Or do you need to see it in your Hardware catalog to be able toinsert it in your hardware configuration? If that is the case. what you need is a Hardware update. Depending on the version of Step 7 in your possession, you mayhave access to this function or not. But if this CPU is recent and its functionnalities are defined for Ste[p 7 v. 5.4 then either you will have to treat it as a lower version, or you will have to purchase the Step 7 v.5.4 upgrade. Look at the following thread, it is very recent and covers almost the same question: /tf/WW/en/Posts/21868#top Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/21/2008 1:12 PM |
|
9/21/2008 11:53 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
closed cause question posted more than once. The active thread with all replies got the subject CPU 414-2XK05-0AB0 GSD fileand is published within the conference SIMATIC S7-400 / S7-400H / S7-400F /FH. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|