2/12/2011 3:46 AM | |
Joined: 10/7/2005 Last visit: 5/23/2024 Posts: 3007 Rating: (1049)
|
Hello Jarek-PL I wonder if your project is set up as a PCS7 type in which case your described "problem" adesired feature. To find out, select the overall project (the "file draw" icon in the left hand window pane ofSimatic Manager), rightclick and open "Object properties" and see if the "Use" drop down box states "PCS7" (and if so, change it back to Step 7 and your problem is solved). I hope this helps |
Cheers |
|
2/12/2011 8:49 AM | |
Posts: 49 Rating: (4) |
Thanks fritz ! I’m changed it and now is active I always have “Use:PCS7” even it wasn’t PCS7 project at all. And in Step7 v5.4 i haven’t such a problem |
Last edited by: Jarek-PL at: 2/12/2011 8:50 AM |
|
This contribution was helpful to2 thankful Users |