6/28/2009 2:38 PM | |
Joined: 1/4/2008 Last visit: 3/19/2025 Posts: 703 Rating:
|
Hello, I suggest to install, the new SP5 for STep7 here. But anyway, you don't need it for the CP443-1, the newFW V2.7 isn't in the HW catalog, there's no additional feature, just correction of some troubles. You could use the V2.6 in the HW configuration. Imho the same is for the CP 1613 A2, you could use the highest you have in the HW catalog (e.g. -3AA00 with the highest SW#). Additional information here. Also you'll need the S7-Redconnect SW. Regards Sydney |
This contribution was helpful to
1 thankful Users |
6/28/2009 3:29 PM | |
Joined: 10/7/2005 Last visit: 3/19/2025 Posts: 3042 Rating:
|
Hello ionut.b just to complement Sydney's reply you asked:
Answer: In HWconfig right click on the PN port of your S7 CPU and select "Insert Profinet system". You'll then be able to add the SCALANCE X202-2IRT to it. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
6/28/2009 5:18 PM | |
Joined: 1/4/2008 Last visit: 3/19/2025 Posts: 703 Rating:
|
Sorry, I forget the last point, thanks fritz for addition. Regards Sydney |
6/30/2009 7:42 AM | |
Joined: 10/7/2005 Last visit: 3/19/2025 Posts: 3042 Rating:
|
Hello again ionut,b
I think it won't workthis way (you are very close to making it work though). Rule number ONE is that there must be only ONE Redundancy Manager in the ring. Your setup will work if enable redundancy manement on only ONEyour 202-2 IRT switch(and nomiate one of the RJ45 ports as part of the ring and one of the FO ports as part of the ring). What I would do though is to have the (ring) FO cables connected to only ONE 202-2 IRT switch andmakeit the RMvia its FO ports (and keep the other 202-2 IRT as a spare). I hope this helps andalso recommend you have a read through the latest Scalance X200 manualwhich has some very good info on redundancy setup possibilities and also the difference between MRP (Media Redundancy protocol - which is what I would use) and HSR setups (High Speed Redundancy, which is actually slower than MRP). I hope this helps |
Cheers |
|
Follow us on