5/14/2020 4:30 PM | |
Posts: 38 Rating:
|
I have built a aquarium light scheduler program ( thanks to your input and from toeternietoe)). it works with a counter and a ramp up/down which generates a specific analog value in AQ1. I would like to store the vale in AQ1 to use as a starting point of that counter. As example: AQ1 is 700 , power goes off and goes on again, it reads 700 and continues the program from there. If the power cut happens during the ramp up, the program would normally restart from 0. Thanks AttachmentBlue Light driver.zip (65 Downloads) |
Last edited by: degregoriis at: 05/14/2020 16:39:02 |
|
5/16/2020 6:18 PM | |
Posts: 38 Rating:
|
can someone explain what it means 'to save voltage fail-safe in the normal way using the program to reuse these values (AQ) when restarting the Logo' ? thanks |
5/16/2020 7:01 PM | |
Joined: 3/27/2009 Last visit: 8/7/2023 Posts: 92 Rating:
|
Hi there , Degregorijs. See your attached diagram if have activated in block 8 & 9 the Retentivity function. See also the JPG file , if you want more information select the help and type retentivity it will explain. AttachmentBlue Light driver retentivity.zip (57 Downloads) |
Last edited by: Peterako at: 05/16/2020 19:02:11 |
|
This contribution was helpful to
1 thankful Users |
5/17/2020 5:50 PM | |
Posts: 38 Rating:
|
thanks Peterarko. So simple yet helpful ! |
Follow us on