2/26/2021 1:28 PM | |
Posts: 1 Rating: (0) |
Hello, I am new here, I have similar request. My application consist of reading data sent by RFID scanner, a motor and few (3 to 4) switches. Please suggest me suitable low cost PLC which can be communicated to RFID reader. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/26/2021 13:56:12New subject after splitting |
|
8/6/2021 8:45 AM | |
Joined: 1/1/2017 Last visit: 7/22/2024 Posts: 331 Rating: (11) |
Hi RusPro, Can you please suggest whether the RFID supports TCP/IP or not! If the TCP/IP protocol is common for all of them then you can go with 1214C CPU along with a managed Scalance for Routing the RFID in a particular Data mode. Regards OmKris |
Follow us on