10/22/2010 5:24 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Fabio; Since you have little experoience with the S7-200, I would suggest looking at simple applications developped by Siemens to give a headstart to programmers using the S7-200 and Logo! controllers: Micro-Automation sets (MAS) for S7-200 and Logo! Controllers: http://support.automation.siemens.com/WW/view/en/34677186/136000&cspltfrm=0&cssw=0&csbinh=8 TheMAS that could interest you at this point is MAS 26: Simple networking and cascading of drives http://support.automation.siemens.com/WW/view/en/21690362 It shows how to develop a water pumping station with 4 drives and motors, so it could be close to your own application. If you are planning to usea cheaper text-based HMI, why don't you look into the TS 200 or TD 400C units that are specifically designed for the S7-200, and are programmed through a wizard in MicroWin. The S7-200 system manual will give you much information in that area (plus all hardware and programming tips for the S7-200): http://support.automation.siemens.com/WW/view/en/1109582 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/22/2010 5:25 PM |
|
Follow us on