11/7/2017 10:16 AM | |
Joined: 7/30/2014 Last visit: 3/16/2025 Posts: 153 Rating:
|
Hello, In our system we have two servers and two engineer stations and 6 operator stations the servers and engineering stations communicate with 9 S7-400 through CP1623 . We did the ghost of one of the two servers and put it in another server. wincc was started on the new server and we got the alarm but all supervision is frozen as if there was no connection to the PLCs. We thought about the MAC address of CP1623 we modified it but the same display is obtained and when we ping the address of one of the PLCs it ping but no data (for the leds of the CP card the green is lit continuously and the yellow flashes but slowly not like the card of the second server). So we are trying to find out if there is a configuration to do or check. see attachment Best regards
Attachmentattachment.docx (81 Downloads) |
Follow us on