5/10/2024 11:09 AM | |
Joined: 9/12/2016 Last visit: 11/11/2024 Posts: 4 Rating:
|
I need to switch on the fly the control mode on Simotion winder axis between V-constsnt to indirect tension control Actually during the transition i feel a web tension release due drop of axis speed. The axis is an axial rewinder system During running in V-constant mode the actual speed is correct and also diameter calculation is right. When i switch to indirect tension control after a few drop of speed , the system restore the right speed and tension in torque limit I set an overspeed by override parameter but sincerely i don't know how remove or reduce this drop of speed during transition Can someone help me? Thanks Luca Moreschi ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2024 06:58:51New subject after splitting |
|
Follow us on