6/10/2011 10:21 AM | |
Posts: 122 Rating: (1) |
Hi everyone, I'm looking at the techincal data for the High Speed DO 16 Module and I understand what output delay time is but I don't know what Switching frequency is. 6ES7322-1BH10-0AA0 Technical data In my case I've got inductive load and according to the data the value for switching frequency is 0,5Hz. It means that the module does something 2 times per second, right? but what exactly does it do? I'm sorry if the question is a bit silly but up to now I was handed the hardware I had to use and now I have to chose it myself and to me, reading the technical data is like reading a hieroglyph. There are so many things I don't understand. Thanks for your help |
6/10/2011 10:35 AM | |
Joined: 10/7/2005 Last visit: 5/24/2024 Posts: 3007 Rating: (1049)
|
Hello Saruca the DQ does not do anything by itself. A switching frequencylimitation of 0.5Hz indicates the fastest permissbleDQ ON-OFF-ON-OFF-ON etc. switching. You need to ensure in your program that you do not try to activate-deactivate the DQ faster than this. Have a look too at the FAQ below which has more on theterminology: What is the meaning of the "Lamp load" specification in digital modules? I hope this helps |
Cheers |
|
This contribution was helpful to3 thankful Users |
6/10/2011 12:02 PM | |
Posts: 947 Rating: (45) |
Hi,Saruca There areseveraltypes ofloads, whichdetermine theswitching frequencyandmaximum allowable currentmodule.Thisresistive, lamp,inductiveandcapacitiveloads.In thedescriptionof the moduleusuallycontains datafor allspecies.Pay attentionto thelinkfromfritz
|
This contribution was helpful to1 thankful Users |