Industry Online Support
Technical Forum
8/10/2011 1:58 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, the TP177 canonly projected with WinCC flexible (current versionWinCC flexible 2008 SP2) If you have the project from the TP170 then you can migrate the project to a TP177 It iswith WinCC flexible very easily. if you start WinCC flexible, then there area point "Open a Protool project" Here some FAQs -> http://support.automation.siemens.com/WW/view/en/18796902 -> http://support.automation.siemens.com/WW/view/en/22001375 -> http://support.automation.siemens.com/WW/view/en/24371560 regards, |
Follow us on