4/15/2013 2:25 PM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Hello, Control loop structures When the mode is changed from speed-controlled to position-controlled mode while the axis is in motion, the equivalent time of the position controller is required to apply the setpoint. The equivalent time is set during configuration in dynamicData.positionTimeConstant (for an electric axis) or in dynamicQFData.positionTimeConstant (for the hydraulic functionality).2.11.5 Dynamic controller data 2.12.3 Example of commissioning a proportional-action controller with precontrol |
With best regards, |
|