8/31/2016 8:11 PM | |
Posts: 4 Rating:
|
Hi, I commissioined the PM240 with CU250s-2DP for hoist application with encoder. our motor rating was 11kw and DBR rated power was 12000w. while in running condition suddenly the drive got off without any fault. At that time operating display R2 parameters displaying the value as 44. please some one can give the solution for the same, Regards PVR AttachmentCU250S-2DP-VECTOR-CONTROL.doc (336 Downloads) |
9/1/2016 2:02 PM | |
Posts: 4 Rating:
|
Terminal 5 i used for on/off Terminal 6 used for direction reverse Terminal 7 used for speed increment Terminal 8 used for speed decrement Terminal 16 used for CDS Bit Terminal 17 not connected, Terminal 16 24v his available and Terminal 17 no voltage. After removing the cable from terminal 16, That time also IN R2 parameter value is showing as 44(Switching on inhibited connect 24v dc to EP(hardware) |
8/14/2018 8:35 AM | |
Posts: 1 Rating:
|
how to solve this problem i am used pm240 and cu240e-2
|
8/14/2018 8:40 AM | |
Joined: 5/12/2006 Last visit: 2/16/2025 Posts: 22541 Rating:
|
check the wiring of the terminals an connect it correctly.
|
Follow us on