Industry Online Support
Technical Forum
6/9/2011 7:27 PM | |
Posts: 3 Rating:
|
I have a 840 DI control and haveset theswivel setting per the manufacture procedure. Attached is the screen shot of the swivel setting page.My machinehas a swivel table. I machined a testsquare in the top plane (A=0.0), then rotated A90. (Front plane) and machined two flats that should match up with the square. Then Rotate C180. (Backplane)and machined two more flats that should match up with the square and flats from the Front plane. Results show that the flats are shifted in the -X direction from Square. Also there is a mismatch between the front and back plane. Is there a swivel setting vector that can be adjusted to correct for the mismatch? I was thinking maybe I3x. Thanks for your help, AttachmentSwivel Setting Screen doc.pdf (105 Downloads) |
6/9/2011 8:22 PM | |
Posts: 2964 Rating:
|
Hello.... Check this Start-up sequence swiveling pdf file will be useful in cross checking informations.... Regards, Ekalavya Attachmentswiv_start_up_uk.pdf (101 Downloads) |
Follow us on