1/30/2020 12:30 PM | |
Joined: 1/18/2020 Last visit: 7/2/2022 Posts: 53 Rating: (0) |
Hi Technodrome, Thanks for the reply. What I actually need is to have some 2nd opinion regarding this matter. Because some other says that it should be enabled rather than disabled. I attached the manual for your reference. AttachmentConfiguration_Symantec_Endpoint_Protection_14_en-US_en-US.pdf (118 Downloads) |
1/30/2020 12:53 PM | |
Joined: 3/14/2008 Last visit: 5/21/2024 Posts: 2067 Rating: (928)
|
Hi, We have a saying when someone has done something wrong which is clearly stated in a manual on how to do this: RTFM (Read The F*cking Manual). This applies for this case....it is clearly stated any other firewall is not recommended and not tested and so not released. During installation of PCS7, PCS7 configures the Windows firewall in order to allow error free operation. If you are going to enable any other firewalls, you must sure know how to configure it and again, the manual states: is not recommended, only Windows Firewall is released. Maybe it will work, maybe it will not. Good luck explaining that to the customer when problems arise and that you have used a firewall not released for PCS7 |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to8 thankful Users |