11/10/2008 9:22 PM | |
Posts: 22 Rating: (0) |
How i can synchronize the OS time with de CPU time. I dont have any extra hardware. this faq https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=22866782&caller=view talks about an CP443...i dont have a hardware with a descripcion like that. I have a CPU 315-2 pn/dp. |
11/11/2008 1:48 PM | |
Posts: 15 Rating: (0) |
Hello dguarello You are on the rigth way, you have the same option at your CPU as the CP in that FAQ has. regards TommyGun |
11/11/2008 1:59 PM | |
Posts: 22 Rating: (0) |
but i dont find the ""Time-of-day Synchronization" tab".... then...where i find that tab in the CPU315-2 PN/DP |
11/11/2008 2:39 PM | |
Posts: 125 Rating: (26) |
Hi, you can define a WinCC-Server as Time-Master: See: "WinCC Information System> Options > Options for Process Control > Time Synchronization" alternative you can use Windows as NTP Server. See Microsoft Support: http://support.microsoft.com/kb/216734/en-us |
11/12/2008 1:16 PM | |
Posts: 22 Rating: (0) |
Yes, but in point 1 talks about a CP443, and i dont have any CP443. I only needthe CPU time synchronized with the OS time. GMT-4 |
11/12/2008 4:14 PM | |
Posts: 3149 Rating: (171)
|
Hi you could check these FAQ as well http://support.automation.siemens.com/WW/view/en/21222026 http://support.automation.siemens.com/WW/view/en/26730707 nemo |
Follow us on