Industry Online Support
Technical Forum
4/9/2012 3:13 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Hello, Simancolic 1. From a similar topics: link1: ...When using the bit alarm procedure or the analog alarms, the "*.EventState" tag is not available by default to provide the group display with the message status... link2: ...Reason: You have placed block symbols in pictures manually, but not all blocks were connected to the appropriate tag structure by using the dynamic wizard "Connect picture block to tag structure"... 2. Do you have a lot of your own script actions in the project? Because it couldn't be PCS script' problem. 3. Look at this Net time consumption thread. As for 4 and 5 maybe you should search not for explanation of an error, but for configuration steps for time synchronisation? What is the principle of time sync. in your system? Did you read PCS 7 - Function Manual Time Synchronisation and PCS7 Compendium Part A - Configuration Guidelines ? Sorry if this is not helpful. |
This contribution was helpful to1 thankful Users |
Follow us on