5/27/2011 1:02 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi makaveli, If you look Master drives pdfthere is lot of deviation if you search from pdf like http://www2.ad.siemens.com.cn/download/Upload/MC/manual/MC%20V2.4.pdf?bcsi_scan_84C833B65C0B3F5A=0&bcsi_scan_filename=MC%20V2.4.pdf """Masking window for homingSetting of a homing point on the fly can be influenced through twomovable windows. The points of reference of the windows are based onthe reference position of U874.2 or the source on U877.3 and definethe permissible deviation between the reference position and themeasured position.The windows allow setting of the homing point to be suppressed if thedeviations are too small or too large.r748.9:(MASTERDRIVES MC) deviation from the synchronizationpoint. Cannot be synchronized, the value is set toNO_SYNCHRONIZATION (= 65535). Should not fluctuateoutside 65515 (-20) and 20.""" I think you might find more for Sinumeric from DocOn Web. http://www.automation.siemens.com/doconweb/ regards Heksu |
Last edited by: Heksu at: 5/30/2011 2:22 PM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
6/2/2011 8:32 AM | |
Posts: 259 Rating:
|
Maybe someone have different info or point of view on this subject. |
Follow us on