3/30/2015 5:14 PM | |
Posts: 21 Rating: (0) |
Hi, I would like to use system diagnostics with FB/FC 49 for Comfort Panels. I am restricted to staying with S7 5.5 PLC software. Does anyone know if this code exists?
http://support.automation.siemens.com/WW/view/en/61910954
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/31/2015 2:29:21 PMNew subject after splitting |
|
2/2/2017 4:19 PM | |
Joined: 11/3/2012 Last visit: 7/23/2024 Posts: 64 Rating: (1) |
Hello, I was also trying the same but not successfull. Then i came to know from the siemens that system diagnostic features only has given to TIA portal. During the selection of PLC one needs to switch on this feature in TIA. But unfortunately the Simatic manager doesn't has this feature.
|
This contribution was helpful to1 thankful Users |
Follow us on