3/2/2009 12:11 PM | |
Posts: 1776 Rating: (95)
|
Hi, delete the dcf file. see FAQ http://support.automation.siemens.com/WW/view/en/26134056 |
This contribution was helpful to1 thankful Users |
3/2/2009 1:58 PM | |
Posts: 157 Rating: (10) |
Dear April, I do what you say, But nothing changed.. please see the picture bellow.. |
8/25/2009 11:18 PM | |
Posts: 2661 Rating: (279)
|
One way is to open another project by double-clicking the project.mcp file of another WinCC project (found in the project root). BTW, is the following thread related to the same problem? Alarm Logging RunTime hangs up (WinCC 7.0) If yes, I think you should delete it. Regards |
Follow us on