8/27/2011 5:31 PM | |
Posts: 151 Rating:
|
hello experts i want to talk with power meter with dlms-cosem protocol. can you help me to start? i search in google but i don't find anything. |
8/29/2011 11:28 AM | |
Joined: 7/18/2011 Last visit: 4/11/2025 Posts: 521 Rating:
|
Hi bermuda, I think you need a protocol gateway like this one http://kalkitech.com/offerings/sync-field_protocol_io_gateways/ Hope this can help a bit, BV |
12/26/2011 3:12 PM | |
Joined: 12/29/2008 Last visit: 9/17/2024 Posts: 24 Rating:
|
Possible solution is to use a gateway between DLMS and Modbus (TCP or RTU). |
Last edited by: LucaM at: 4/28/2017 9:42:59 AM |
|
11/28/2013 1:18 PM | |
Posts: 3 Rating:
|
Hello Bermuda Our SYNC 2000 can be used to connect the DLMS meter(where the meter can be connected directly to the RS485 port on our SYNC 2000 protocol converter, or if multiple meters needs to be read, they can be multidropped in daisy chain) to the Modbus master device We have successfully completed numerous projects integrating DLMS Meters to the master devices(which are on Modbus, IEC61850, DNP3, etc) Here is the link of case study of the recent project which we completedhttp://www.kalkitech.com/documents/SYNC%202000%20Protocol%20Gateway%20V2_Case%20Study.pdf, where we integrated DLMS meters to IEC61850 SICAMPAS system Best Regards, Gautam Bhat |
Last edited by: O_Moderator at: 11/28/2013 1:48 PMcontact data deleted |
|
Follow us on