2/17/2014 8:26 AM | |
Joined: 10/7/2005 Last visit: 3/18/2025 Posts: 3042 Rating:
|
Hello 7gallon you are not missing anything, the "problem" is that open communications via T-Blocks are NOT supported via a CP343-1 (see also What differences are there between the Industrial Ethernet CPs of SIMATIC S7-300? on what connections are possible). If you want to use the CP343-1 for the comms you willneed toconfigure the connection the good old fashion way inNetpro. I hope this helps |
Cheers |
|
Follow us on