5/30/2012 10:35 AM | |
Posts: 1547 Rating:
|
Hello, i don't know if you have seen this sample transferring data (with FC5 "AG_SEND" and FC6 "AG_RECV") with variable message lengths via the TCP protocol who solves your problem. |
5/30/2012 10:43 AM | |
Posts: 487 Rating:
|
The link goes to a empty search page |
5/30/2012 10:54 AM | |
Posts: 3093 Rating:
|
Hello Aikona, just try this link. Regards, Kaulquappe |
5/30/2012 12:10 PM | |
Joined: 3/24/2006 Last visit: 11/17/2024 Posts: 58 Rating:
|
Hi Kaulquappe this example is for CP341 , s7300 CPU this AG_RECV function for s7-300 and S7-400 has same inputs and outputs, I did try this block also with s7 300 and CP341 Lean but it did not work. in this configuration with lean CP341 i could not read any data until my receive lenth was > 200 BYTE ... but in this case i only receive a data of 200 byte at once and i could not receive even one single message .. it sound also stange for me..:) but may miss something after some trials on cp341 i decided to try cp441 and CPU s7-400 it works better (can receive differrent lenth of data) but still have some offset and stiil do not know the lenth.. thank you |
5/30/2012 1:08 PM | |
Joined: 3/24/2006 Last visit: 11/17/2024 Posts: 58 Rating:
|
I will Try it Thankyou |
5/30/2012 1:41 PM | |
Posts: 3093 Rating:
|
Hello Ozi, here is a thread in which this matter was discussed. Regards, Kaulquappe |
Follow us on