6/30/2014 1:03 PM | |
Posts: 1368 Rating:
|
Hello, in the TCON_Param UDT, there is a Parameter "active_est ". FALSE: passive connection establish |
6/30/2014 3:17 PM | |
Posts: 1368 Rating:
|
Which blocks do you use on PC/PLC side? Comesthe error code "80A7" from "TCON"? This means here"communication error- TDISCON is called before TCON ends". |
6/30/2014 3:54 PM | |
Joined: 3/17/2014 Last visit: 8/31/2021 Posts: 31 Rating:
|
No, sorry I started using TSEND_C as it looks easier all-in-one function. Hope the screenshots make the problem clearer. ss1 is showing the current configuration for TSEND_C. ss2 is showing the TSEND_C ladder code. ss3 is showing how the variables look when I try to connect to the PC by rising edge in CONT input. I am trying to connect to a PC with a simple TCP server on the same port as it is configured in TSEND_C to connect to. Thanks for your help AttachmentScreenshots.zip (447 Downloads) |
7/1/2014 10:47 AM | |
Posts: 1368 Rating:
|
do you know this FAQ: http://support.automation.siemens.com/WW/view/en/67196808? |
Last edited by: Pittiplatsch at: 7/1/2014 10:51 AM |
|
7/1/2014 11:47 AM | |
Joined: 3/17/2014 Last visit: 8/31/2021 Posts: 31 Rating:
|
Hi, I agree with everything you said, that is how I am doing it and this is why it looks so weird. However there are a couple of details that may give us some hints:
Can this be causing any issue? Thanks for your help!
|
7/1/2014 12:46 PM | |
Posts: 1368 Rating:
|
Hello, could the firewall cause this problem? Can you switch of the firewall on PC and tray again with PLC = active? Just one more idea... |
This contribution was helpful to
1 thankful Users |
Follow us on