8/29/2016 1:47 PM | |
Posts: 1 Rating:
|
Hi, I want to create a network infrastructure with the TCP connection to interfacing the PLCs (see attachment). The CPU Master is a 317-2EK14-0AB0 V 3.2 and 10 CPU Slave are S7300 CPU family with CP343 LEAN aboard. The communication with the slaves are with TCP protocol and not S7 connection, it's possible? AttachmentPROJECT.pdf (57 Downloads) |
Last edited by: matteo.florian at: 8/29/2016 1:48:34 PM |
|
9/18/2016 12:03 AM | |
Joined: 7/19/2016 Last visit: 6/18/2018 Posts: 28 Rating:
|
Yes, use Open User Communication You have blocks on Step7 and TIA portal to do the communication |
Follow us on