11/23/2018 7:05 AM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating:
|
Hi, S7 400 PLC(CP443-1) communicating with three s7 300 PLCs(CPU with PN) using TCP/IP. We are configured all s7 300 PLC as a unknown project. 1. Process01 - Communication ok 2. Raw01 - Communication ok 3.Tai01 - Communication ok if i try to read 52 bytes from s7 300 plc. but i have to read 190 bytes from third party PLC. If i try to read more than 52 bytes i am getting status code: 19 & 4 and getting error 1. anybody have idea to sort out the problem. Thanks in Advance AttachmentDEVA.zip (49 Downloads) |
Regards \ Sankar |
|
11/23/2018 8:41 AM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating:
|
Hi, The links are correct between s7 400 and all other three s7 300 PLCs. |
Regards \ Sankar |
|
11/23/2018 9:08 AM | |
Joined: 12/13/2011 Last visit: 10/1/2024 Posts: 146 Rating:
|
Hi. I would try a maximum block of 32 bytes |
11/23/2018 9:10 AM | |
Joined: 12/2/2010 Last visit: 4/2/2024 Posts: 61 Rating:
|
Hi, As per the document maximum 400 bytes for s7 400 PLC |
Regards \ Sankar |
|
11/23/2018 9:17 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, so you're still in limit so? Sry maybe Kaulquappe can look to that error code, you're use AG blocks? Post zip-ed screenshots how you did cfg. What is that 3-rd party system? Sry if I missunderstand your info, problem is with SEND or RECV from that 3-rd party partner? Update: eeeeeh now I see that ZIP file and this is like Javier stated, S7 communication... |
Last edited by: Duris_I at: 11/23/2018 9:22:57 AMWith best regards... |
|
Follow us on