6/11/2009 8:26 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, I understood that you use the native TCP protocol (not ISO on TCP). TCP is stream based and you must take this into account, especially if the messages have a variable length. Here an example. http://support.automation.siemens.com/WW/view/en/19033929 Intesting also in that example is that on the same connection, you may only start the send only once till you get done. Here another FAQ on the usage of AG_LSEND http://support.automation.siemens.com/WW/view/en/24693800 |
Best regards |
|
Follow us on