8/27/2015 9:43 PM | |
Posts: 439 Rating:
|
Hello, One of my customer try to access a basic panel through a router. 6AV6647-0AK11-3AX0 SIMATIC HMI KTP400 BASIC COLOR PN https://support.industry.siemens.com/cs/us/en/ps/6AV6647-0AK11-3AX0 This HMI is connect with a S7-1200 on an unmanaged ethernet switch. So, both of them are behind the router. It's posible for him to connect with the S7-1200 through the router, but it's not possible for him to connect with the basic panel. Both of them are configure in the project to go through the router and both of them are in the same IP address range which is 10.225.171.X. When he connect directly into the unmanaged switch, he is able to connect to both device. He tried to switch the IP address of the S7-1200 and the HMI and he is still only able to access to the S7-1200. Here is my question: Is there any specific TCP/IP port he needs to forward on the router to connect to the basic panel? Best regards, Hugo P.S.: I opened a support request before. So if I get news, I will let you know. |
Last edited by: HugoDufour1 at: 8/27/2015 9:48:52 PM |
|
9/2/2015 3:00 PM | |
Posts: 439 Rating:
|
Here is some interresting links: Which ports are used by WinCC Advanced, WinCC Runtime Advanced, WinCC Runtime Professional, Basic Panels, Comfort Panels, Panels and IPC? http://support.automation.siemens.com/WW/view/en/80917729 https://support.industry.siemens.com/cs/ww/en/view/109096785/72538448011
Which ports are used by WinCC flexible? http://support.automation.siemens.com/WW/view/en/24534065 Which ports are used by the various services for data transfer by means of TCP and UDP and what should you watch out for when using routers and firewalls? http://support.automation.siemens.com/WW/view/en/8970169 |
Follow us on