7/31/2018 5:42 AM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
Hi This is a testing program for menu navigation in TDE. In the LSC simulation I can navigate between pages and change the counter by Cursor keys (C1, C2, C3, C4) easily. But in the real testing these Cursor keys work differently; For both LOGO BM and LOGO TDE I have to press ESC + C keys . without holding ESC it doesn't work . AttachmentTDE.zip (146 Downloads) |
Last edited by: DL110 at: 7/31/2018 5:43:48 AM |
|
7/31/2018 5:54 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32887 Rating: (4066)
|
This is normal and is so, since it's the LOGO! and / or the TD (E) is produced. So nothing new. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 129.pdf (169 Downloads) |
Last edited by: ixo65 at: 7/31/2018 6:04:38 AMattachment |
|
This contribution was helpful to1 thankful Users |
7/31/2018 7:46 AM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
|
Follow us on