Industry Online Support
Technical Forum
3/26/2013 9:59 PM | |
Posts: 28 Rating:
|
Dear All, I've a problem with Technology object "Command Table". Reading the manual, variables such as Position, Velocity andDuration (among others)are accesible and can be modified during the program execution. As you can see in the attached document, these variables are present in the DB related to the command table but only NextStep, StepCode and Type variables are accesible when I'm writing the program. I need to modify these variables during program execution but I'm not able to access them. I'll be grateful for your suggestions.. Attachmentexample.pdf (289 Downloads) |
3/26/2013 10:02 PM | |
Posts: 28 Rating:
|
Problem solved !!!!! |
3/26/2013 10:41 PM | |
Joined: 9/23/2005 Last visit: 2/3/2023 Posts: 4178 Rating:
|
Hi, what happned?
|
Denilson Pegaia |
|
Follow us on