12/2/2016 10:37 AM | |
Posts: 5 Rating:
|
Arfter instlaling, When i try to connect to my opc server using opc scout or other clients I can see tha the OPCServerDown is true and i cant seee items. what can be the problem? Attachment2016-12-02 10_20_09-apps1r2 ( 192.168.18.22, 192.168.3.2, 192.168.14.22, 10.0.20.jpg (307 Downloads) |
12/5/2016 3:30 PM | |
Posts: 5 Rating:
|
Yes, I use opc UA server, form TCSB (teleocntrol server basic) tags delivered by the opc server are about server 8see attachment) but not about stations connected that are a plc 7-S1200 what do you mean with system topology? the computer where runs the client and the server it's the seme ( with 2008 server r2 sp1 64 bit) Attachment2016-12-05 15_26_50-apps1r2 ( 192.168.18.22, 192.168.3.2, 192.168.14.22, 10.0.20.jpg (159 Downloads) |
12/5/2016 3:32 PM | |
Posts: 5 Rating:
|
overwiew of the server
Attachment2016-12-05 15_31_07-apps1r2 ( 192.168.18.22, 192.168.3.2, 192.168.14.22, 10.0.20.jpg (220 Downloads) |
6/1/2018 12:25 AM | ||
Joined: 7/4/2014 Last visit: 3/8/2024 Posts: 1 Rating:
|
, I am having same issue as you with OPCServerDown=True. Please, could you explain how did you insert Autostart of TCSB on Simatic.net? Thanks! |
|
4/24/2019 9:07 PM | |
Joined: 1/14/2019 Last visit: 3/1/2025 Posts: 10 Rating:
|
Please explain IN DETAILS how did you do it. I use Windows 10. Thanks. |
5/7/2020 11:32 AM | |
Joined: 1/14/2019 Last visit: 3/1/2025 Posts: 10 Rating:
|
Answer, please? |
Follow us on