Industry Online Support
Technical Forum
1/27/2011 10:56 AM | |
Posts: 376 Rating: (57) |
Hello together, the software TeleService S7 V6.1+SP2 is current not released for Windows 7. The drivers TS Adapter and TS Adapter IE are yet not adapted for the Windows 7, 32 Bit system. So there are problems with this software constellation. In the next future a new service pack (SP3 ?) will come for TeleService V6.1+SP2. This Service Pack will support Windows 7, 32 Bit version. A later version of TeleService also will be compatible for Windows 7, 64 Bit system. If you have the problem “you see not the register Modem in PC/PG interface” with TeleService V6.1 and Windows 2000 or Windows XP, please install the Service Pack 2 for the software TeleService V6.1. You find the Service pack 2 here: http://support.automation.siemens.com/WW/view/en/10805406/133100 Best regards Gucci |
4/15/2011 10:02 AM | |
Joined: 1/15/2010 Last visit: 10/22/2022 Posts: 19 Rating: (0) |
I have the same problem.. Windows 7 OS Step7 v5.5 Teleservice v6.1 + SP2 So, we have to wait for SP3.. Thanks Samuele |
4/15/2011 11:59 AM | |
Joined: 4/24/2006 Last visit: 5/22/2024 Posts: 8656 Rating: (1152) |
Hello, Here is the solution: TeleService V6.1 incl. SP3 Best regards, Wizard |
5/17/2011 4:54 PM | |
Joined: 1/15/2010 Last visit: 10/22/2022 Posts: 19 Rating: (0) |
Thants a lot.. I'm going to try it! |