4/6/2006 2:51 PM | |
Joined: 9/27/2005 Last visit: 4/26/2024 Posts: 203 Rating: (32) |
Hallo roemsen, I have no experience with LOGO! but I know, that there exist some LOGO!-applications-examples. https://www.automation.siemens.com/microset Maybe it is helpful for you. Greetings Morten |
4/7/2006 2:55 AM | |
Posts: 62 Rating: (19) |
Greetings roemsen, I think the S7-200 would be a better choice for this project. When I start LOGO Softcomfort and start dropping in analog inputs, it wouldn't go beyond 8 connections. That's 4 LOGO mains and 16 RTD Modules. Dollar wise (ouch!) that's going to hurt. An S7-224 will handle up to 7 thermocouple modules at 4 points per. That's closer, so with 2 PLC and 8 thermcouple modules, you're there. Just watch the power budget so the PLC will have enough +5 and + 24 to power the rest on the modules. You might also look at the 3RS10/3RS11, https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&objid=20369781&DataKey=20369781&treeLang=en Best Regards, Thumper |