6/22/2020 12:01 PM | |
Joined: 5/6/2019 Last visit: 9/12/2023 Posts: 78 Rating:
|
Hallo All, Recently sometimes I started to get failure with PLC, when it has changes in its configuration. For eg when new gsdml file is loaded or when new plc program is loaded, when telegram is changed etc. The plc diagnostic buffer has the following error Temporary CPU error: User programmed STOP request in FB 32781 affecting OB 123 execution HW_ID= 52 Internal address details: Caddr=16#0000071A Then if I reset the memory and load the PLC again I get the memory card evaluation error. And finally I have to format the memroy card. What could be the reason for this errror? AttachmentFB32782.pdf (96 Downloads) |
6/24/2020 12:15 PM | |
Joined: 5/6/2019 Last visit: 9/12/2023 Posts: 78 Rating:
|
Now I have the event details.This time I was trying to load another PLC program. I am using TIA 16. Is tis somehow realted to sw version also? AttachmentFB32782_Diagnostics.txt (121 Downloads) |
6/28/2020 11:14 AM | |
Joined: 11/1/2017 Last visit: 8/20/2023 Posts: 4 Rating:
|
Hallo. Did you try to actualise the programm? |
This contribution was helpful to
1 thankful Users |
6/29/2020 12:25 PM | |
Joined: 5/6/2019 Last visit: 9/12/2023 Posts: 78 Rating:
|
Thank you. This worked |
Follow us on