Industry Online Support
Technical Forum
2/17/2011 3:45 PM | |
Posts: 2 Rating:
|
We've got an application on site that was developed using WinCC Flex 2008 SP1, on a TP1500 Basic PN HMI. The HMI progect was developed using this version of WinCC Flex and has been working on site at our customer's for a number of months now. Recently I've updated to WinCC Flex 2008 SP2, and since then I have made a couple of changes to the alarm text (the screens themselves haven't been edited). I Visited site today to download these changes, and was informed that I needed to update the existing HMI's version of WinCC Flex / Firmware to match what I was using on my PC. After doing this and downloaded the project to the HMI again, and after doing so the text I am seeing on the HMI and project it's self seems to have increased in size for some reason. Is there a resolution setting that I would need to make to the HMI, or is there a known issue here? I can't seem to understand how this would have happened. AttachmentWinCC FLex 2008 SP1 vs SP2.zip (21 Downloads) |
2/17/2011 3:54 PM | |
Joined: 4/29/2010 Last visit: 9/21/2023 Posts: 1557 Rating:
|
Hello, i think this is the solution and the cause of your attitude: Why are fonts and objects shown shifted on a PC Runtime system or operator panel? best regards |
2/17/2011 4:53 PM | |
Posts: 2 Rating:
|
Thanks for your help, my development PC was indeed set to large DPI font size. |
Follow us on