1/30/2020 1:55 PM | |
Posts: 6 Rating:
|
Attached a printscreen of prg. Try too explain your idea aboyt analog idea. Tried to add an analog flag but didnt manage to write to it. I have the right version of Logo with web server. Have already made some tests with web editor and it works fine with simple digital/analog signals showed by animation,thats no problem. I want to display same info in webserver as on Logo Display,thats case! Thanks for help! AttachmentBild Logo.docx (44 Downloads) |
1/30/2020 2:02 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
Please upload your Programm as zip file. A screenshot is not helpfull. |
1/30/2020 2:12 PM | |
Posts: 6 Rating:
|
Here comes a zip!
AttachmentProject_200123-delay off Q4.zip (37 Downloads) |
1/30/2020 3:11 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
I make you an example with your projekt. One moment please. |
1/30/2020 3:25 PM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
In attachment the example and your file with the extension through Parameter-VM-Mapping. In order to be able to display and set the values of the counters and their switch-on limits, the parameters must first be transferred to the VM memory. These values require 4 bytes or a double word. A double word in the VM memory has in the LOGO! the designation "VD". You must upload the LWE Project to the LOGO!. This requiers a mSD Card in the LOGO!. AttachmentIVJS_LWE.zip (47 Downloads) |
This contribution was helpful to
1 thankful Users |
1/31/2020 6:57 AM | |
Joined: 12/18/2014 Last visit: 12/5/2023 Posts: 31552 Rating:
|
Hello IVJS, you're welcome... |
Follow us on