9/28/2016 2:02 PM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello Murof, The example is almost the same as I am using now. The difference that I see is only in HW and ConnectionType (0E - 14 I have 0B - 11 TCP/IP). Sending works. By receiving is status for TCON 7002 and it is Busy. Parameters for Scalance are the same as in instructions for example. Attachment54361177_SMS_SCALANCE_M_DOC_V10_en.pdf (70 Downloads) |
Follow us on