3/28/2020 12:40 PM | |
Posts: 3 Rating:
|
I have also a little problem with the min. and max range. The minimum and maximum value stays both gray so I can't alter them. Someone an idea? Please see attached picture. To use the recipes, I made a User_data_type. In a DB I created an array in which I use the User_data_type. Next, I created 10 recipes with each 100 Data records (limitation of basic panel). The elements in the recipes are tagging to the DB. What do I have to change so I can alter the minimum and maximum values? Best regards, Richard ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/30/2020 10:41:05New subject after splitting |
|
2/2/2021 10:18 PM | |
Joined: 7/3/2019 Last visit: 8/31/2023 Posts: 1 Rating:
|
Hallo, Kun je me vertellen hoe je dit hebt opgelost? Ik kan het ook niet.
|
Follow us on