7/10/2014 1:30 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
Hello, the SSP V2.6 SP2 is only installable on Win7 32bit System in the additional mode. you have 2 ways: download the latest STARTER version with all SSP and install the SSP during the STARTER installation. modify the setups.ini of the SSP end add the Win7x64 support. But this is on you own risk! Regards Christoph |
This contribution was helpful to1 thankful Users |
7/10/2014 2:53 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
Windows XP Mode is not supported ;) So if you have a problem with this then do not contact the support ;) |