6/3/2011 8:54 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Hello playerslight, have you seen the link shown in attachment? Best regards O_Moderator |
6/3/2011 9:00 AM | |
Posts: 1064 Rating: (72) |
Yes i have and use it all the time but i think what they are asking for is a link to unanswered posts |
This contribution was helpful to1 thankful Users |
6/3/2011 9:07 AM | |
Joined: 10/7/2005 Last visit: 5/22/2024 Posts: 3005 Rating: (1048) |
Dear all the unansweredposts links that MavEriclisted are just the tip of the Iceberg. You can already easily find outwhich posts never received a reply by going to the product conference and clicking on heading in the"Replies" column which will sort them in descending order and all posts with "-" replies surface to the top. |
Last edited by: fritz at: 6/3/2011 9:08 AMtypos Cheers |
|
6/3/2011 9:10 AM | |
Posts: 691 Rating: (36) |
Its the responsibility of the Thread starters to remind once more. Simply posting anything and left , this isn't fair.
An Expert can't tell anything. If your CPU is not working because of a pin of the backplane connector got broken, and you are posting that its not working. Then what the Expert will do. If the Expert is sitting over a place and the problem is reported at the far distant place, then what Expert will do. He can't see whether the Pin is broken or not. For that case the client has to ask for Siemens Service Engineer. I repeat once more, the Thread starters must remind to the Forum that they are still in problem. Simply digging in the History of the Forum and taking out unused stuffs |
This contribution was helpful to1 thankful Users |
Follow us on