8/10/2018 7:36 PM | |
Posts: 4 Rating:
|
I need to measure the a (high) frequency input (on I4) transmitted by a (24V) flow meter in a water circuit. In order to display the flow, i tried both a threshold trigger and an up/down counter. When testing with a manual set Input, I found that the threshold trigger outputs the frequency as put in the Input, but the Up/Down counter gives always lower number. The difference exceeds 10% for lower frequencies but reduces on higher frequencies. The difference is so high, i can only assume my flow chart is wrong. Any idea? AttachmentMEASURE FREQUENCY threshold trigger VS up_down counter.zip (47 Downloads) |
8/11/2018 9:40 PM | |
Posts: 4 Rating:
|
Yes thanks a lot you are right. No difference with an 'live' input. regards, JOhan |
This contribution was helpful to
1 thankful Users |
Follow us on