1/13/2023 1:07 PM | |
Joined: 4/20/2010 Last visit: 1/17/2023 Posts: 38 Rating:
|
Hello, I confirm, this is still not possible in TIAv17 Upd4 However, to bypass this issue, we have developped an "addin" that allows to do that : By selecting the DB you need to re-numbered, then activate the addin Then you can select the first DB number, and the addin will re-numbered all DB Here is the addin. Please replace .txt by .addin And place it in the followinf folder : Hope this will help people ! Seb AttachmentNumber_block_V17 Numerotation dans une plage.txt (185 Downloads) |
Follow us on