8/20/2021 4:27 PM | |
Joined: 11/4/2011 Last visit: 8/28/2025 Posts: 276 Rating:
|
I'm not the one to comment all the points you gathered, there for sure is something about all the things you listed, but about this point:
Just contact tech support via support request and address one issue per request (to not mix things up), and you'll have an expert that looks at it and addresses the issue to developement (if needed). Just because there's no external bug tracker doesn't mean that bugs are not tracked at all. |
Last edited by: daviso at: 08/31/2021 09:34:32 |
|
This contribution was helpful to
3 thankful Users |
9/6/2021 10:32 AM | |
Joined: 7/16/2021 Last visit: 11/30/2022 Posts: 20 Rating:
|
Hello Weekly update. This weeks submission: Last weeks submission status (2.7.1 - undo history being dropped on project save):
|
9/7/2021 3:29 PM | |
Joined: 7/7/2010 Last visit: 9/5/2025 Posts: 16061 Rating:
|
You are not likely to get any traction on the Undo history loss at project save. This has been this way for as long as I can remember and is the same in every windows program I regularly use except perhaps Notepad++, and I'm completely sure about that one. The broad assumption is you only save work when you have not need to undo anything. Perhaps you need a "save + undo history" option added for those times when you need to shut down (rather than allow hibernate), but do not want to lose the undo history. I know I'd appreciate having the undo history persist between saves in certain situations, but at some point, the undo history is from project start and undo back to that point would be unwieldy to implement and use.
|
science guy |
|
9/8/2021 11:41 AM | |
Joined: 7/16/2021 Last visit: 11/30/2022 Posts: 20 Rating:
|
Hello For this weeks submission (3.2 Broken HMI build system), they are requesting some samples to help to trace the problem (which might prove to be a little bit difficult). If you encountered the problem and want to help to solve it, details are in the separate WinCC forum post. |
9/15/2021 12:04 PM | |
Joined: 7/16/2021 Last visit: 11/30/2022 Posts: 20 Rating:
|
Weekly update: This weeks submission: Very simple sample project demonstrating the issue submitted. Hope this one should be pretty straight-forward to pin down. Last weeks submission status (3.2 Broken HMI build system):
|
Follow us on