11/3/2012 7:17 PM | |
Posts: 10 Rating:
|
Need I to install all previose updates to, or only last? Regards. |
11/5/2012 3:22 PM | |
Posts: 168 Rating:
|
Where to find this update? Can't find it when using the search function. I do need to update as soon as possible, it crashes several times per day for me |
11/5/2012 3:32 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
Just a couple threads down in the list from this thread: /tf/WW/en/Posts/82442#top The link shows up in German. Just select your language (I selected English) and it downloaded and installed in English just fine. |
science guy |
|
11/26/2012 3:22 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
For crashes like this, send to Support Requestso they can make sure it gets fixed in the programming of the portal. Crashes affect everyone. In the meantime while you wait, try creating a new plc within your project, copy tags/dbs, OBs, and everything except the SCL blocks. Get it to compile using the compile rebuild all (you have tried that already right?) with simple stub code or temporarily deleting calls to scl blocks. Once your project compiles, copy one block at a time and compile / rebuild all blocks until you find the block that causes it to crash. Delete that block and see if it still crashes when compiling. If not, copy it back from the original project, then open it in the editor to see what might cause it to crash. I have an scl FB that has several embedded block calls inside one line (and some automatic type conversions). It crashes every time. For this one block (it was important for the project), I copied all the external FB code into that block, added explicit type conversions, and it compiled. The big one was the explicit type conversions that resulted in too many nested calls. I do not know the limit, but somehow it went too far. Maybe this is useful for your SCL blocks. |
science guy |
|
Follow us on