1/13/2013 7:53 PM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello rdoliveira, Yes you are right, you can't install the downloaded SP2 directly in a Win7 64 bit OS. You may need to order any of the below mentioned which costs a nominal fee or contact your local Siemens representative Contacts Worldwide STEP 7 Basic V11, Trial License (6ES7822-0AA01-0YA7) or STEP 7 Professional V11,Trial License (6ES7822-1AA01-0YA7)or SIMATIC WinCC Basic V11 SP2, TRIAL (6AV2100-0AA01-0AA7) or SIMATIC WinCC Comfort/Advanced V11 SP2, TRIAL (6AV2102-0AA01-0AA7) or SIMATIC WinCC Professional V11 SP2, TRIAL (6AV2103-0AA01-0AA7) But I have heard this in forum though I don't have a personal experience on it. 1. Download from Siemens site SP2. 2. Unpack to folder without installation = Extract files to full package 3. Open and edit SIA.INI = add ; to line in TERM section 4. Install In this way you will install SP2 on 64 bits without need DVD. Share your success if u r trying the same. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
1/14/2013 6:18 PM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello rdoliveira, Download Service Pack 2 for STEP 7 V11from here Download Service Pack 2 for WinCC V11from here |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
1/19/2013 8:18 AM | |
Posts: 1 Rating: (0) |
64bit 可以安装SP2 |
Follow us on