2/11/2015 5:05 PM | |
Posts: 1 Rating:
|
When using TIA Portal V11, I'm having trouble going online with a S7-1200 PLC through Ethernet IP communications. I was given an existing project to open, but when I right click on the device and select "Go Online" no configured access nodes appear under this controller (see slide 1 of attachment). However, when I go to: Online -> Accessible Devices, both the PLC and HMI appear. I am also able to ping both the PLC and HMI IP addresses. Any suggestions?
AttachmentS7-1200_CantGoOnline_2015_02_11.pdf (213 Downloads) |
2/11/2015 6:40 PM | |
Posts: 784 Rating:
|
Hello, First,select suitable PG/PC interface. Best regards...... |
Follow us on