5/8/2014 4:46 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hallo, normely, you can use both version V12 and V13 on the same PC. Check whether you have a full or an upgrade version of STEP 7 (TIA Portal) V13 in refer to the articel no. By an upgrade version the installation of V12 is neccessery. See also the FAQ: http://support.automation.siemens.com/WW/view/en/57775228 But in your case I recommend to deinstal STEP 7 V12 complete. See in this case the FAQ: http://support.automation.siemens.com/WW/view/en/76325723 After complete deinstallation try to install the V13 again. Mit freundlichem Gruß |
Follow us on